Boiler Guide's Product of the Month

01/11/2016

Grundfos circulator range

The ALPHA3 has just been announced as the Product of Month with Boiler Guide who provide householders with a simple way to find a recommended boiler installer. Given that the ALPHA3 offers best-in-class efficiency and if used in conjunction with the ALPHA Reader and Installer app can help to simplify hydronic balancing – it is a worthy winner.

With an energy efficiency index of just 0.17, the new ALPHA3 is the most energy-efficient circulator in its class, it analyses the pattern of use and automatically adjusts the power output down to as little as 3W when the demand is low, offering a huge energy saving compared to standard pumps.

Put simply, this new ALPHA3 redefines what a small domestic circulator can do. Filled with useful features and robust hardware, the circulator raises the bar for efficiency and reliability in domestic circulators, even in the toughest systems

Read more about boiler guide's product of the month here.