BG customers notice the Grundfos difference

18/06/2012

British Gas - ALPHA2

It was back in March this year that British Gas took the important decision to only offer their customers the ALPHA2 which is an award winning variable speed energy efficient circulator from Grundfos Pumps.

British Gas and Grundfos Pumps have built up a strong business partnership in recent years and are both united in their determination to deliver to their customers the highest levels of comfort, in the most energy efficient way.

Today this means that potentially thousands of British Gas customers a month are already benefitting from the energy savings of up to 75% to 80% offered by a Grundfos ALPHA2 as opposed to having to wait for legislation to kick in.  This legislation will take the form of the EuP Directive that covers Energy using Products and will demand that only the most energy efficient products can be fitted from 1st January 2013.