Condensate sorted with Grundfos CONLIFT

25/02/2016

CONLIFT range

Condensate can be a real problem in certain situations, for example in applications that include dehumidifiers, air conditioning systems as well as in terms of modern condensing boilers. At Grundfos we have provided a solution to these issues for many years with our range of Grundfos CONLIFT pre-assembled lifting stations.

This family offers 3 models, an entry level CONLIFT1 LS, the CONLIFT1 and CONLIFT2. The CONLIFT1 LS has a few less features, but still offers a range of benefits including easy installation, low noise operation and superior reliability.  A big plus for these units is that they are also suitable for connecting to a domestic boiler PRV.  This means they are able to handle high temperature (≤90°C) inflows for up to 5 minutes. All models in the CONLIFT range have been tested and confirmed suitable for connection to the discharge from a domestic (<40kW) condensing boiler Pressure Relief Valve (PRV).

The motor/pump unit can turn 180° on the tank which increases the flexibility of the installation process, a situation which is enhanced by the four symmetric well-sized inlets
that means the unit can be connected from any direction.  In addition this compact range can be installed either as floor standing or as wall mounted units. 

Find out more about the CONLIFT family by visiting the product page


    Facebook Twitter LinkedIn