Energy savings + CO2 savings = Grundfos Pumps

05/04/2016

Energy savings + CO2 savings = Grundfos Pumps

Energy as well as CO2 savings have become increasingly important targets to realise reductions in for many businesses today. There are occasions when it is possible to simultaneously achieve these ambitions and this is true in the instance of pumps, as they provide the potential to deliver major savings on both fronts.

So how can you achieve this? Well at Grundfos Pumps, we offer a range of diagnostic tools including an Energy Check or Pump Audit that will help to establish the current pump system performance. In fact, this is what we found out when we recently worked with a range of clients to see how we could help them. This included a brewery where we delivered an energy saving of 75% simply by identifying and changing key pumps; a chassis manufacturer that benefitted from a pump upgrade and saved 51%, while a power plant saw a saving of 50% from taking Grundfos’ advice.   

This means that regardless of if the priority is cost reduction, CO2 savings, ROI, a water usage reduction or just simply to get advice on your current installations, Grundfos have the tools, expertise and integrity to help you to achieve your ambitions.

To find out more click here and see how you could benefit.