Grundfos extend CONLIFT family

16/12/2013

CONLIFT LS

The CONLIFT family has recently had a new model added to it and now besides the CONLIFT1 and CONLIFT2 there is a new cost effective entry level model the CONLIFT1 LS.

This new model has a few less features than the CONLIFT1, but still offers a range of benefits including easy installation, low noise operation and superior reliability.

All CONLIFT models are supplied with an integrated NC/NO contact and cable so that if the overflow switch detects a high water level this can be used to switch off the boiler. CONLIFT2 options include an acoustic alarm in case of a high water condition. They also have a selector switch with additional options.

The advanced design of the CONLIFT range means they work automatically when condensate enters the collection tank from an appliance. The units then lift the condensate up to 5m in height and across a distance of several metres to the required drainage point. Another plus is that these units require minimal maintenance.

 

Find out more about the different options available with the new CONLIFT family  


    Facebook Twitter LinkedIn Technorati