Grundfos extends MAGNA3 range

06/05/2014

MAGNA3 range

When Grundfos Pumps introduced the updated MAGNA3 range of commercial circulators in 2012 the family was quickly recognised as offering ‘best in class’ in terms of energy efficiency. This new generation of state-of-the-art circulator pumps built on the excellent reputation that MAGNA established when it was introduced in 2001.

Today the extended range offers an extra 25 models, meaning that the MAGNA3 offers a circulator range that can support light, medium and large commercial heating, air conditioning and cooling systems, domestic water systems, ground-source heat pump systems and solar heating systems.

With its simple installation wizard the MAGNA3 has been designed for easy and intuitive installation. It comes with a high-resolution colour display and once the pump is turned on, the Assist™ software immediately guides the installer through set-up. With many integral features including AUTOADAPT that helps optimise energy usage in conjunction with the FLOWADAPT and FLOWLIMIT control features that allow a maximum flow limit to be set, which means the pump continuously monitors the system.

Offering complete control over every aspect of the pumps performance, Grundfos developed the innovative Grundfos GO control software. From the user-friendly interface on a smart phone or iPod Touch, you can monitor, set and control MAGNA3 as well as other Grundfos e-pumps.

With so much attention on both the bigger and smaller details, this pump family is an important step forward in pump engineering. A point that has been proven by the MAGNA3 winning a series of design and engineering awards.  

View MAGNA3 product brochure


    Facebook Twitter LinkedIn Technorati