Have you got the energy to make savings?

02/02/2018

Have you got the energy to make savings?

Saving energy as well as CO2 have become increasingly important targets for many companies. It will come as a pleasant surprise to realise that there are occasions when it is possible to achieve these ambitions and pumps are often a major contributor, as they provide the potential to deliver major savings on both fronts.

So how can you achieve this?  Well at Grundfos Pumps, we offer a range of diagnostic tools including an Energy Check that will help to establish the current pump system performance.  This is exactly what we found out when we recently worked with a range of clients to see how we could help them. This included a brewery where we delivered an energy saving of 75% simply by identifying and changing key pumps; a chassis manufacturer that benefitted from a pump upgrade and saved 51%, while a power plant saw a saving of 50% from taking Grundfos’ advice.   

This means that regardless of if the priority is cost reduction, CO2 savings, ROI, a water usage reduction or just simply to get advice on your current installations, Grundfos have the tools, expertise and integrity to help you to achieve your ambitions.