MAGNA3 all systems GO

02/11/2012

MAGNA3 launch

The new MAGNA3 range of innovative, energy efficient circulators from Grundfos Pumps is already proving to be a very popular choice. This could be because of the wide range of commercial applications that it can be used in that includes: heating systems, air con and cooling systems, domestic water systems, ground source heat systems and solar heating systems.

Or is this success down to the fact that the MAGNA3 range incorporates many standard settings – some of which are new and unique - including AUTOADAPT which finds the optimum setting. FLOWLIMIT that limits maximum flow and FLOWADAPT that offers the combined benefits of AUTOADAPT and FLOWLIMIT. Perhaps it’s because of the extended range of single and twin head options up to 18m head and flows of 70m3/h (140m3/h for twin head versions) and a system pressure of between 6 to 16 bars. In addition these pumps can cope with liquid temperatures from -10 degrees C to +110 degrees C making them the perfect fit for both heating and cooling applications.

To stay in control at all times, access to these new MAGNA3 pumps is available via the new Grundfos GO intuitive mobile handheld remote control. So monitoring, checking the operational parameters, changing the settings and getting and storing reports is now easy with this the industry’s most advanced mobile pump control solution. So now it’s all systems GO.

For more information about the MAGNA3 click here