More Grundfos booster sets gain WRAS approval

04/04/2014

Hydro GTI booster sets

In 2013, Grundfos Pumps attained WRAS (Water Regulations Advisory Scheme) full product approval status for their range of Hydro MPC E/F/S booster sets.

This scope covered Grundfos Hydro booster families that comprise of between two to six pumps, are up to a 16 bar PN rating and pump models up to CR(E)90.

Approval is only granted following rigorous mechanical testing and ensures that these complete booster sets comply with the various strict byelaw regulations and requirements as they currently exist in the UK.

Now the range of Grundfos Hydro GTI booster sets, have also attained full WRAS approval status. This range has been specifically designed to meet many boosting demands including: smaller commercial applications, residential homes, potable water, wash-down systems and irrigation systems. Sets are also suitable for Category 5 applications (as defined by Water Regulations Backflow Prevention) and are suitable for use in both new and retrofit applications, making them perfect for many different applications.

Grundfos have built up a great reputation in supplying booster sets to the highest standards. With all the elements relating to the design, engineering and build combining to deliver to the most exacting standards, these sets are perfect for a wide range of applications from hotels to education establishments, high rise developments to industrial demands as well as within the water utility industry itself.

So now you have even more reasons to choose Grundfos.

 


    Facebook Twitter LinkedIn Technorati