Need a Perfect Fit?

07/09/2015

Need a Perfect Fit?

Grundfos today offer a range of options that are designed to make the decision of which domestic circulator pump to choose a more straightforward one.

These include the Grundfos UPS2 15-50/60, a compact, high efficiency, replacement for the Grundfos UPS 15-50/60 circulator pumps. Made in the UK, the UPS2 is available as a complete pump or as pump head (PH) only for easy replacement. Models for larger applications are also available.

The Grundfos ALPHA2L is designed to circulate water in domestic heating systems with constant or variable flows and in systems with variable temperature. These high efficiency circulators can be installed in central heating and primary hot water circuits up to 35kW and offer many advanced features.

At the top of the list is the latest ALPHA2 version D circulator the most energy efficient domestic circulator available to the market. This pump offers all the benefits of the ALPHA2L plus the patented AUTOADAPT setting and an LED display. New for the 2015/16 heating season, ALPHA2 models now also benefit from an extra robust start-up dry run protection and Summer Mode functions, factors that add to this pumps already impressive service life.

Grundfos are currently running a range of merchant based promotions that offer pump purchasers the opportunity to win a number of rewards. This includes the chance to be one of 50 UK professional heating engineers who will get the chance to fly by luxury private jet to the Grundfos Danish HQ for a VIP trip. Click here to find out more.