SP pumps now the best in class

01/08/2011

SP pumps

The Grundfos SP family of submersible pumps have always been renowned for their efficiency and reliability.

Made entirely of corrosion resistant stainless steel, these pumps are ideal for a wide variety of applications that includes groundwater supply, irrigation, groundwater lowering, pressure boosting as well as a range of industrial applications.

With their state-of-the-art hydraulic design and built to deliver optimum efficiency during periods of peak demand, the SP pumps already provide low long-term costs and high operating reliability regardless of the application. And the best just got better with the opening of a new test facility at the SP factory In Denmark that now means that Grundfos can offer the option of having these SP pumps tested to ISO 9906 Grade 1 and 2 standards. The test plant cost almost 4m Euros and was three years in the planning. Pumps up to 8m and with an output of 250kW and a voltage of 1,000 can now be tested.

The ability to deliver to such strict standards is something that is required by many customers around the world, especially those involved in wastewater applications.

Visit SP product page


    Facebook Twitter LinkedIn Technorati