The Grundfos UPS2 will fit your needs

12/02/2014

UPS2 pump and pump head

Introduced in 2013 the new Grundfos UPS2 is the ideal replacement for the popular UPS 15-50 and 15-60 circulator families and they are rapidly becoming a firm favourite and are suitable for use in both new and replacement scenarios.

Additionally, the Grundfos UPS2 pump head is proving to be very popular in tight-fit applications and restricted spaces e.g. in boilers or pre-plumbed cylinders.

Designed to meet the strictest energy requirements, the UPS2 is a compact, newly engineered pump that is built in the UK and offers many benefits:

  • fully compliant with the energy demands of the 2013 and 2015 EuP legislation
  • one single model replaces 5m and 6m versions of the UPS
  • the cable gland is the same as the UPS, minimising wiring time
  • dimensions are almost identical to the UPS.

In instances where the pump base is in good condition, only the pump head needs to be replaced and the new UPS2 pump head is compatible with all ALPHA, ALPHA Pro, ALPHA+ and UPS 15-50 and 15-60, 5m and 6m variants.

All this adds up to the UPS2 delivering a versatile generation of domestic circulators that will fit your needs.

Vist the UPS2 product page


    Facebook Twitter LinkedIn Technorati