UPS2 – the big story

04/11/2014

UPS2 25-80 and 32-80

Grundfos are delighted to introduce the latest additions to their UPS2 circulator family of British built pumps the UPS2 25-80 and 32-80. These pumps have been specially designed to augment the current range and provide 8 metre options.

Offering a number of distinct benefits, these pumps deliver enhanced efficiency that meets the latest EuP/ErP requirements, while the dimensions will ensure straightforward replacement with older UPS generations.

These circulators have new more powerful motors and improved hydraulics which makes them perfect for use in a range of large domestic and small commercial applications as they can deal with a flow rate of 5.7 m3/h and a system pressure up to 10 bar.

With over 16 million electronically controlled Grundfos circulators installed globally choosing a UPS2 option big or small, makes perfect sense.

For more information about the UPS2 25-80 and 32-80 please click on this link to visit the product page.


    Facebook Twitter LinkedIn Technorati