Water supply
Wastewater
Agrigulture
Industrial solutions
More Industrial solutions
Service & support
There is now less than a year to go to the 1st January 2013 EuP/ErP deadline that will change the standalone circulator market in Europe forever. This EU Directive on energy using products (EuPs) sets strict new requirements for energy efficiency that includes domestic and light commercial circulator pumps.
At Grundfos we are not just ready – we’re way ahead. The Grundfos ALPHA2 and MAGNA circulators have met the EuP demanded requirements for many years. For example the ALPHA2 runs on as little as 5W, and in 2008 was the double winner of the Energy+ Award for best energy-efficient circulator. And with more than two million units produced and sold since the market introduction in 2007, it has proved its reliability around the globe. The same can be said about the Grundfos MAGNA for commercial building applications that was introduced to the market in 2001. This reliable pump uses up to 70% less energy than other standard standalone circulators.
So don’t have to wait for legislation to come into force before you make the energy efficient choice, just opt for the Grundfos ‘A’ team today.
The rules on small and medium circulator use change on the 1st January 2013, make sure you are ready to meet the new EuP legislation.
The Grundfos MAGNA and ALPHA2 meet the EuP requirements today.