Grundfos IE5 motors are officially super

03/01/2017

IE5

As a pioneer in the pump industry, Grundfos are delighted to introduce one of the world’s most efficient motors, the new MGE with IE5 efficiency. By selecting a pump with these motors incorporated will mean a 10% energy saving as well as up to a 25% reduction in payback time.

Not only are these motors capable of delivering an unprecedented level of performance, but their ground-breaking efficiency far exceeds the forthcoming IE3 legislative standards, but actually meet the strictest IE5 criteria – the highest energy efficiency level for electrical motors. New generation Grundfos MGE motors – from 0.25 kW to 11 kW – now qualify as capable of attaining this ‘super’ status.

The key to these MGE motors unparalleled performance lies in their state-of-the-art intelligent solutions as these adapt to the surrounding system and, coupled with the high-efficiency IE5 motor, drive down energy consumption.

With their integrated frequency converters, these motors combine the accumulated pump experience of Grundfos into their dedicated control software. This combination of pump and customisable software optimises your system’s performance for any load point, delivering an unsurpassed reduction of energy consumption.