Meet the new Grundfos team line-up

11/09/2018

Domestic heating circulators

At Grundfos we understand that for you to be successful, you need the right team behind you, so we are delighted to announce our new and improved domestic circulator line-up who are ready to meet all the challenges of the heating season.

Replacing ALPHA2L, the new ALPHA1 delivers the highest efficiency on the market, whilst the new ALPHA3 delivers the same high efficiency but also includes wireless hydraulic balancing and set-up direct to your smartphone, now without the need for a separate ALPHA Reader. (The new ALPHA1 is also available as a stainless steel “N” version for DHW applications).

The star signing and superseding the market leading UPS2, is the new UPS3 is built on a platform that has already proven in millions of boilers. The UPS3 has maintained the features that you liked, such as: manual deblocking, robust start-up and ceramic shaft / bearings, but has also added a new plug, increased efficiency. Plus, it will allow for a faster first-time fix, as it replaces many OEM boiler pumps. You just scan an old pump with the Grundfos GO Replace app to confirm if the Grundfos UPS3 can be used.   

:: Get the know the new line up