Staying in control at Glastonbury

06/05/2019

Staying in control at Glastonbury

As music festivals go, they don’t get bigger or better than Glastonbury. The logistics of putting on an event for over 200,000 people is mindboggling and ensuring the availability and accessibility of sufficient clean water is just one aspect. This involved Grundfos Pumps being asked to advise the organisers in relation to further optimising their system.

After a site survey, attention switched to improving the overall control and efficiency of the booster units.  This is an important aspect as energy use and sustainability are always high on Glastonbury’s agenda.  Coming up with a bespoke solution to this unique requirement, Grundfos put forward a coordinated approach that involved several suggested activities. This involved the upgrade of the pump motors to more energy efficient versions, the incorporation of a new precision dosing system and a remote monitoring system that would mean a significant improvement in data exchange. 

These changes are overarched by the new Grundfos remote monitoring system which will mean that all aspects of the network can be accessed and interrogated 24/7, with an instant inbuilt alarm to advise of any issues.  

Grundfos Pumps will not feature on the Pyramid Stage or be listed on a programme, but they are very proud to be playing a small role in delivering an important, if rather taken for granted element - water.