Built to order

11/09/2018

Offsite Build

Offsite build is today recognised as providing a vital solution that is helping to overcome a range of issues currently being experienced, for example, the industry wide skills shortage. These pre-engineered solutions tick all the boxes in terms of the coordination of a range of elements from planning and design, through to fabrication, the actual assembly of components, plus all required testing.

At Grundfos, we are seeing these requests coming from a range of diverse areas such as: larger building projects, industrial solutions as well as from the water industry, all of which can benefit from having packaged sets arrive on site complete with all the necessary pumps, piping, valves, instrumentation and controls. 

Selecting a partner who has the capacity, knowledge, expertise as well as all the necessary accreditations to deliver all the stages within the process is key. This is where the 12,000m2 Grundfos manufacturing plant in Sunderland adds value, as it is a recognised centre of manufacturing excellence that offers customers design, build, assembly, test and distribution from under one roof, making this a streamlined and very cost-effective option. 

There is a real future for these systems that have the flexibility to consistently deliver a complete solution to a myriad of demands so get ready, get set and get Grundfos.

:: See examples of our offsite build solutions