GO Replace app

Download the GO Replace app

The GO Replace (available on both iOS and Android), uses a look-up database to confirm if their new UPS3 domestic circulator will be a suitable replacement.

You can check this out by simply scanning the old pump and in seconds you’ll have your answer – quickly and conveniently.  

Download the app for iOS here: App Store

Download the app for Android here: Google Play

How to use the GO Replace app

Once you have downloaded the app, you are just a few steps away from a straightforward and reliable answer that will advise you as to if this is one of the many thousands of pumps that Grundfos can offer you a replacement for. 

This is how it works:

1. Take a picture using the app

2. Enter the product number (if the app recognises the number when the pictures is taken it is automatically inserted, otherwise this can be input manually)

3. Select the application where the pump is to be installed – i.e. inside a boiler, an underfloor heating installation, a solar application

4. The app will show whether Grundfos can offer a suitable replacement5. If required, the app

can generate a report.

During initial use, the app will request you to provide your name, company name and address

and to accept an End User License Agreement (EULA), terms and conditions and the Grundfos

Privacy Policy.

All this means that the Grundfos UPS3 offers the opportunity to be a one-stop domestic circulator

pump replacement in many OEM type applications such as in the case of boiler repairs.